SABRE On screen keyboard Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE On screen keyboard Issue

Jump to solution
1,765 Views
lijothomas
Contributor II

Hi all,

Completely new to the iMX world, procured a SABRE board for our development activity.

Ported linux successfully using LTIB and Yocto environments .

The on screen board functionality is not working,  tried to add lot of stuffs but nothing works.

Could anyone suggest any methods to get the on screen keyboard for the SABRE platform.

Thanks in Advance !!!!!!

Regards

Lijo Thomas

Labels (1)
0 Kudos
Reply
1 Solution
1,647 Views
art
NXP Employee
NXP Employee

Try the latest L3.14.28 Yocto Linux BSP by Freescale, available for free download on the i.MX6 SABRE SD Software&Tools web page (check the "Board Support Packages" section):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

Everything works well there.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,648 Views
art
NXP Employee
NXP Employee

Try the latest L3.14.28 Yocto Linux BSP by Freescale, available for free download on the i.MX6 SABRE SD Software&Tools web page (check the "Board Support Packages" section):

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Design_Too...

Everything works well there.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------