SABRE Board for Smart Devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SABRE Board for Smart Devices

跳至解决方案
2,174 次查看
rs1932
Contributor I

In the reference SABRE Board for Smart Devices, there is a provision for 1GB with 4 chips. Is it possible to only populate 2 of those for a total of 512MB? Would that work or do some changes need to be made in the schematics?

Also, it looks like the dual lite will work with no changes to the board schematics?

Thanks for any help or pointers.


RS

标签 (6)
0 项奖励
回复
1 解答
1,894 次查看
Yuri
NXP Employee
NXP Employee

  The i.MX6 MMDC supports DDR data bus width of x16, x32 or x64 bits.
On the SABRE Board for Smart Devices x64 configuration is applied.
Generally it is possible  to use only one DDR part (D[0-15]) or two
parts (D[0-31]). DDR initialization should be changes to reflect
bus size in  MDCTL[DSIZ].

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,895 次查看
Yuri
NXP Employee
NXP Employee

  The i.MX6 MMDC supports DDR data bus width of x16, x32 or x64 bits.
On the SABRE Board for Smart Devices x64 configuration is applied.
Generally it is possible  to use only one DDR part (D[0-15]) or two
parts (D[0-31]). DDR initialization should be changes to reflect
bus size in  MDCTL[DSIZ].

0 项奖励
回复