SABRE Board for Smart Devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SABRE Board for Smart Devices

Jump to solution
2,201 Views
rs1932
Contributor I

In the reference SABRE Board for Smart Devices, there is a provision for 1GB with 4 chips. Is it possible to only populate 2 of those for a total of 512MB? Would that work or do some changes need to be made in the schematics?

Also, it looks like the dual lite will work with no changes to the board schematics?

Thanks for any help or pointers.


RS

Labels (6)
0 Kudos
Reply
1 Solution
1,921 Views
Yuri
NXP Employee
NXP Employee

  The i.MX6 MMDC supports DDR data bus width of x16, x32 or x64 bits.
On the SABRE Board for Smart Devices x64 configuration is applied.
Generally it is possible  to use only one DDR part (D[0-15]) or two
parts (D[0-31]). DDR initialization should be changes to reflect
bus size in  MDCTL[DSIZ].

View solution in original post

0 Kudos
Reply
1 Reply
1,922 Views
Yuri
NXP Employee
NXP Employee

  The i.MX6 MMDC supports DDR data bus width of x16, x32 or x64 bits.
On the SABRE Board for Smart Devices x64 configuration is applied.
Generally it is possible  to use only one DDR part (D[0-15]) or two
parts (D[0-31]). DDR initialization should be changes to reflect
bus size in  MDCTL[DSIZ].

0 Kudos
Reply