SABRE Board for Smart Devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE Board for Smart Devices

ソリューションへジャンプ
2,159件の閲覧回数
rs1932
Contributor I

In the reference SABRE Board for Smart Devices, there is a provision for 1GB with 4 chips. Is it possible to only populate 2 of those for a total of 512MB? Would that work or do some changes need to be made in the schematics?

Also, it looks like the dual lite will work with no changes to the board schematics?

Thanks for any help or pointers.


RS

ラベル(6)
0 件の賞賛
返信
1 解決策
1,879件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The i.MX6 MMDC supports DDR data bus width of x16, x32 or x64 bits.
On the SABRE Board for Smart Devices x64 configuration is applied.
Generally it is possible  to use only one DDR part (D[0-15]) or two
parts (D[0-31]). DDR initialization should be changes to reflect
bus size in  MDCTL[DSIZ].

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,880件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The i.MX6 MMDC supports DDR data bus width of x16, x32 or x64 bits.
On the SABRE Board for Smart Devices x64 configuration is applied.
Generally it is possible  to use only one DDR part (D[0-15]) or two
parts (D[0-31]). DDR initialization should be changes to reflect
bus size in  MDCTL[DSIZ].

0 件の賞賛
返信