Running Java apps on Linux 2.6.35 on SABRE tablet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running Java apps on Linux 2.6.35 on SABRE tablet

ソリューションへジャンプ
2,924件の閲覧回数
winstonrodrigue
Contributor IV

Dear Pals,

 

         I m a new bee linux developer. I have a project where i have to run java aps on SABRE tablet having iMX53 (ARMv7) running linux 2.6.35 kernel.

  I have installed LTIB in ubuntu 9.04. and i know how to compile n build the kernels and rootfs. I need to know what are the steps involved in running a java app on this iMX53 system.

     How to install JRE in the iMX53 Linux 2.6.35.

     How to develop a simple touch application for this tablet.

     How to run that java app on the target system.

     What should be the requirements of Host system to develop java apps for SABRE tablets.

Thanks And Regards,

     Winston.

ラベル(1)
タグ(3)
1 解決策
2 返答(返信)
2,295件の閲覧回数
Yuri
NXP Employee
NXP Employee
2,294件の閲覧回数
winstonrodrigue
Contributor IV

Hi Yuri Muhin . . ..

     Thanks a lot for your valuable reply.

Using your resources I could compile one simple GUI app using ecj compiler . And Run it successfully.

 

Theres another question..

Is it possible to design GUI for the same platform using Netbeans...

If yes how do I configure my Netbeans IDE for ARMv7 (IMX53) Platform ?

Regards,

Winston Rodrigues

0 件の賞賛
返信