Repetitive Kernel logo in sabresd kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Repetitive Kernel logo in sabresd kernel

ソリューションへジャンプ
2,576件の閲覧回数
mrigendra_chaub
Contributor III

Hi I am using sabresd reference board, and android O source from nxp.

While booting up I am seeing linux tux penguin logo at top right corner.

I am seeing 4 penguins, but I want to show only one,

1. How can I do that.

2. How can i change the position of it, like if I want to put it into middle of the screen.

Regards,

Mrigendra Chaubey

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
2,290件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mrigendra Chaubey,

The penguin (named Tux, and the Linux mascot) is shown on the Kernel splash screen and one is shown for each core, so you are most likely running the i.MX6Q.

There are a couple of threads where the topic of changing the Kernel Splash screen is discussed, as for example:

https://community.nxp.com/message/960347?commentID=960347#comment-960347

There is not a simple guide on how to do this but perhaps this or other threads on the community may be of help.

Regards,

元の投稿で解決策を見る

1 返信
2,291件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mrigendra Chaubey,

The penguin (named Tux, and the Linux mascot) is shown on the Kernel splash screen and one is shown for each core, so you are most likely running the i.MX6Q.

There are a couple of threads where the topic of changing the Kernel Splash screen is discussed, as for example:

https://community.nxp.com/message/960347?commentID=960347#comment-960347

There is not a simple guide on how to do this but perhaps this or other threads on the community may be of help.

Regards,