Repetitive Kernel logo in sabresd kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Repetitive Kernel logo in sabresd kernel

Jump to solution
2,586 Views
mrigendra_chaub
Contributor III

Hi I am using sabresd reference board, and android O source from nxp.

While booting up I am seeing linux tux penguin logo at top right corner.

I am seeing 4 penguins, but I want to show only one,

1. How can I do that.

2. How can i change the position of it, like if I want to put it into middle of the screen.

Regards,

Mrigendra Chaubey

Labels (1)
0 Kudos
Reply
1 Solution
2,300 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mrigendra Chaubey,

The penguin (named Tux, and the Linux mascot) is shown on the Kernel splash screen and one is shown for each core, so you are most likely running the i.MX6Q.

There are a couple of threads where the topic of changing the Kernel Splash screen is discussed, as for example:

https://community.nxp.com/message/960347?commentID=960347#comment-960347

There is not a simple guide on how to do this but perhaps this or other threads on the community may be of help.

Regards,

View solution in original post

1 Reply
2,301 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mrigendra Chaubey,

The penguin (named Tux, and the Linux mascot) is shown on the Kernel splash screen and one is shown for each core, so you are most likely running the i.MX6Q.

There are a couple of threads where the topic of changing the Kernel Splash screen is discussed, as for example:

https://community.nxp.com/message/960347?commentID=960347#comment-960347

There is not a simple guide on how to do this but perhaps this or other threads on the community may be of help.

Regards,