Reg. Mfg tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reg. Mfg tools

2,631 Views
jalathimohan
Contributor I

Hi, What are the pre-requisites for using Mfgtools-Rel-1.6.2.042.?

Do we need to install any framework? The tool crashes after selecting the USB ports tab through Options->Configuration->USB Ports in a Win7 PC

0 Kudos
Reply
3 Replies

2,236 Views
SergioSolis
NXP Employee
NXP Employee

I had this problem too a while ago , and it was fixed by updating the .NET framework of windows 7. Can you try updating windows 7 to the latest date?

0 Kudos
Reply

2,236 Views
lategoodbye
Senior Contributor I

Hello Jalathi,

it's a software bug in the program. In the case a USB root in the mentioned tab contains no elements, the programm dies of a null pointer dereference.

I've send a patch to Freescale last year, but i don't know in which version this fix is included. Unfortunaly i don't have this patch anymore.

As a quick solution for your problem try to use another PC.

0 Kudos
Reply

2,237 Views
Yuri
NXP Employee
NXP Employee

  Perhaps the problem relates to USB3 options. The MFG  on the Web does not support USB3.

Some MFG problems relate to the general USB3 support under OS and issues may be

solved, when USB3 ports are disabled in Win 7 / 8. 

0 Kudos
Reply