i.MX6S SDXC support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6S SDXC support

1,473 次查看
Paul_Kang
NXP Employee
NXP Employee

Hello,

According to our i.MX6S RM, it says i.MX6S can support SDXC as like below.

Up to 832 Mbps of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode

But, I wonder if our BSP can support SDXC as well and there is no problem to support over 1TB capacity as well. According to SDXC spec, it seems to support up to 2TByte but I am not sure if our BSP or file system can have limiation to do it.

Best regards,

Paul

标记 (2)
1 回复

1,217 次查看
SergioSolis
NXP Employee
NXP Employee

Hello Paul,

Yes, the i.MX6 supports SDXC, as well as the BSP supports it.

0 项奖励
回复