Reference clock of DLL (Delay Line) in Read Path in DDR mode.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Reference clock of DLL (Delay Line) in Read Path in DDR mode.

跳至解决方案
1,385 次查看
takayuki_ishii
Contributor V

Hello community,

I have one question about reference clock(ipp_card_clk_in) frequency of DLL (Delay Line)

if uSDHC is in DDR(dual data rate) mode.

I think that

   * 50MHz in SD3.0 DDR mode

   * 52MHz in EMMC4.4 DDR mode

So reference clock period of ipp_card_clk_in are 

   * 20ns = 1/50MHz in SD3.0 DDR mode

   * 19.2ns = 1/52MHz in EMMC4.4 DDR mode.

It is not 100 or 104MHz(10 or 9.62nsec) in each DDR mode.

Is it correct?

Best regards,

Ishii.

标签 (1)
0 项奖励
回复
1 解答
1,266 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

regarding these questions - yes your understanding for them all is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,267 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

regarding these questions - yes your understanding for them all is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,266 次查看
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your quick response.

I will answer it to my customer.

Best regards,

Ishii.

0 项奖励
回复