Reference clock of DLL (Delay Line) in Read Path in DDR mode.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Reference clock of DLL (Delay Line) in Read Path in DDR mode.

Jump to solution
1,355 Views
takayuki_ishii
Contributor V

Hello community,

I have one question about reference clock(ipp_card_clk_in) frequency of DLL (Delay Line)

if uSDHC is in DDR(dual data rate) mode.

I think that

   * 50MHz in SD3.0 DDR mode

   * 52MHz in EMMC4.4 DDR mode

So reference clock period of ipp_card_clk_in are 

   * 20ns = 1/50MHz in SD3.0 DDR mode

   * 19.2ns = 1/52MHz in EMMC4.4 DDR mode.

It is not 100 or 104MHz(10 or 9.62nsec) in each DDR mode.

Is it correct?

Best regards,

Ishii.

Labels (1)
0 Kudos
Reply
1 Solution
1,236 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

regarding these questions - yes your understanding for them all is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,237 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ishii

regarding these questions - yes your understanding for them all is correct.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,236 Views
takayuki_ishii
Contributor V

Hello Igor,

Thank you for your quick response.

I will answer it to my customer.

Best regards,

Ishii.

0 Kudos
Reply