Recommended connection when not used LICELL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Recommended connection when not used LICELL

Jump to solution
1,460 Views
ko-hey
Senior Contributor II

Hi all

Let me confirm about recommended connection for LICELL in PF3000.

1.

I found the following document which describe about recommended connection for PF0100.

http://cache.freescale.com/files/analog/doc/app_note/AN4717.pdf?fasp=1&WT_TYPE=Application%20Notes&W...

Can the recommended connection also apply for PF3000 ?

2.

According to the Table 1 of AN4717, NXP recommended user to connect "Bypass with 0.1 μF" when not used LICELL.

In my understanding this mean "Bypass with 0.1 μF to ground".

Is it correct ?

Ko-hey

Labels (3)
0 Kudos
Reply
1 Solution
1,331 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, you're right, just bypass through 0.1 μF to ground

View solution in original post

0 Kudos
Reply
2 Replies
1,332 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, you're right, just bypass through 0.1 μF to ground

0 Kudos
Reply
1,331 Views
ko-hey
Senior Contributor II

Hi

Thanks!

Ko-hey

0 Kudos
Reply