Recommendations for write leveling delay values on i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Recommendations for write leveling delay values on i.MX6Q

跳至解决方案
2,808 次查看
jschoen
Contributor III

Should the WRITE_LEVELING delay register values be set greater than the worst case delay value measured across boards?

The documents and discussions usually defer to using a model of the design to set the WRITE_LEVELING delay, but from our measurements using the DDR Stress Test, there is significant deviation board to board which may not align with a modeled design center.  Proposing to set delays in the shape of the average line but offset to where they are beyond the worst case delays

标签 (1)
0 项奖励
回复
1 解答
2,633 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jschoen

procedure normally to average them

Best regards

igor

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,633 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jschoen

I am afraid it is not true to use worst case delay value measured

across boards. Ideally board should use own  WRITE_LEVELING delay register values.

Difference accross boards may be caused by impedance mismatch or board noise.

One can recheck with sect.3.4 DDR routing rules IMX6DQ6SDLHDG

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,633 次查看
jschoen
Contributor III

Igor,

I found this related post : https://community.freescale.com/thread/319387

It suggests sampling 5-10 boards and get calibration values.  Then balance the write leveling values (normally average them).  This is essentially what we've done....obtained calibration values for a sample build of same board design.

Is it recommended to average the write leveling value or use the worst case delay value?

Thanks.

Joel

0 项奖励
回复
2,634 次查看
igorpadykov
NXP Employee
NXP Employee

Hi jschoen

procedure normally to average them

Best regards

igor

0 项奖励
回复