AUDMUX internal to internal port connectivity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AUDMUX internal to internal port connectivity

Jump to solution
2,187 Views
saurabh206
Senior Contributor III

Hi

I want to set AUDMUX internal to internal port connectivity.

What changes required in imx_audmux_config.

I have gone through the AUDMUX IMX6DQRM :Chapter 16.

Thanks

Saurabh

Tags (1)
0 Kudos
Reply
1 Solution
1,864 Views
saurabh206
Senior Contributor III

Hi Jimmy

This issue is already fixed.

Now AUDMUX internal to internal port connectivity is working perfectly.

Thanks

Saurabh

View solution in original post

0 Kudos
Reply
5 Replies
1,863 Views
宗標廖
Contributor V

Hello, Saurabh

Could you tell me your workaround?

Thank you very much!

ZongbiaoLiao

0 Kudos
Reply
1,863 Views
saurabh206
Senior Contributor III

Hi

ZongbiaoLiao

I need to do following modification.

- Continues clock generation for SSI.

- Correct imx_audmux_config for Internal mode

- Register Dummy recording driver

And used ALSA aplay/arecord command to start playback and capture.

Thanks

Saurabh

0 Kudos
Reply
1,864 Views
saurabh206
Senior Contributor III

Hi

Is there any update?

I have implemented but I am getting silence data.

0 Kudos
Reply
1,864 Views
jimmychan
NXP TechSupport
NXP TechSupport

would you show more details about what you want to do?

and what you have done at this moment?

what BSP are you using?

0 Kudos
Reply
1,865 Views
saurabh206
Senior Contributor III

Hi Jimmy

This issue is already fixed.

Now AUDMUX internal to internal port connectivity is working perfectly.

Thanks

Saurabh

0 Kudos
Reply