Read IMX8X internal temperature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Read IMX8X internal temperature

跳至解决方案
1,656 次查看
AFR89
Contributor III

Hello,

 

I would like the know if it's possible to read the internal temperature of the IMX8X without passing by the SCFW? (sc_misc_get_temp)

 

Best regards

Alexandre

0 项奖励
回复
1 解答
1,651 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

 

>if it's possible to read the internal temperature of the IMX8X without

>passing by the SCFW? (sc_misc_get_temp)

 

no. Also for reading temperature one can look at sect.2.9 Thermal  i.MX Linux Reference Manual​

 

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,652 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

 

>if it's possible to read the internal temperature of the IMX8X without

>passing by the SCFW? (sc_misc_get_temp)

 

no. Also for reading temperature one can look at sect.2.9 Thermal  i.MX Linux Reference Manual​

 

Best regards
igor

0 项奖励
回复