Read IMX8X internal temperature

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Read IMX8X internal temperature

Jump to solution
1,664 Views
AFR89
Contributor III

Hello,

 

I would like the know if it's possible to read the internal temperature of the IMX8X without passing by the SCFW? (sc_misc_get_temp)

 

Best regards

Alexandre

0 Kudos
Reply
1 Solution
1,659 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

 

>if it's possible to read the internal temperature of the IMX8X without

>passing by the SCFW? (sc_misc_get_temp)

 

no. Also for reading temperature one can look at sect.2.9 Thermal  i.MX Linux Reference Manual​

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
1,660 Views
igorpadykov
NXP Employee
NXP Employee

Hi Alexandre

 

>if it's possible to read the internal temperature of the IMX8X without

>passing by the SCFW? (sc_misc_get_temp)

 

no. Also for reading temperature one can look at sect.2.9 Thermal  i.MX Linux Reference Manual​

 

Best regards
igor

0 Kudos
Reply