Re: UART pins condition during power on reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Re: UART pins condition during power on reset

796 次查看
ban45
Contributor III

Hello,

NVCC is a power-up.
POR_B then releases the reset.
It is in the reset state after the power is turned on.
Is the pin in that case undecided?

best regard

0 项奖励
回复
1 回复

789 次查看
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

   Use table "Functional Contact Assignments", column "Out of Reset Condition"
of the Datasheet for pin states after power is up, POR is negated.

 

Regards,
Yuri.

0 项奖励
回复