Re: UART pins condition during power on reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: UART pins condition during power on reset

833件の閲覧回数
ban45
Contributor III

Hello,

NVCC is a power-up.
POR_B then releases the reset.
It is in the reset state after the power is turned on.
Is the pin in that case undecided?

best regard

0 件の賞賛
返信
1 返信

826件の閲覧回数
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

   Use table "Functional Contact Assignments", column "Out of Reset Condition"
of the Datasheet for pin states after power is up, POR is negated.

 

Regards,
Yuri.

0 件の賞賛
返信