Re: UART pins condition during power on reset

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: UART pins condition during power on reset

777 Views
ban45
Contributor III

Hello,

NVCC is a power-up.
POR_B then releases the reset.
It is in the reset state after the power is turned on.
Is the pin in that case undecided?

best regard

0 Kudos
Reply
1 Reply

770 Views
Yuri
NXP Employee
NXP Employee

@ban45 
Hello,

   Use table "Functional Contact Assignments", column "Out of Reset Condition"
of the Datasheet for pin states after power is up, POR is negated.

 

Regards,
Yuri.

0 Kudos
Reply