RX FIFO ERROR while both camera streaming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RX FIFO ERROR while both camera streaming

2,837 次查看
vimalan_93
Contributor I

Hi,

I am using the linux kernel 4.14.78 from sumo bsp in imx8m EVK (REV-B4) board. I can able to successfully stream the cameras in both minisas connectors individually. But when i tried to stream the both cameras simultaneously i received the RX_FIFO_OVERFLOW error. In NXP release notes they already mentioned about this issue i also attached the screenshot here for your referance. so, Is there any workaround for this issue.

When did you planned to deliver the next release?

Thanks

vimal.

标记 (2)
0 项奖励
回复
2 回复数

2,700 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not have that type of information. I apologize for the inconveniences this could you.

Best regards,

Diego.

0 项奖励
回复

2,700 次查看
vimalan_93
Contributor I

Hi Diego Adrian Cuevas

I need to use both the cameras simultaneously, but when i tried to do the same i faced this RX_FIFO_OVERFLOW error from one of the camera very frequently. How to solve this issue? Any comments would really helpful for us.

Thanks,

Vimal.

0 项奖励
回复