How use max9286 in the imx6q?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How use max9286 in the imx6q?

1,179件の閲覧回数
Nian8113
Contributor I

Hi everyone,

  I referenced the max9286 patches.

iMX6DQ MAX9286 MIPI CSI2 720P camera surround view solution for Linux BSP

  Then, I can find 4 devices (like /dev/video0, /dev/video1...) in the system.

  But I wish max9286 can combination of 4 cameras to one device (only /dev/video0) in the system.

  Have any idea or suggestion?

  I use L4.1.15_2.0.0-ga BSP.

Thanks.

ラベル(5)
0 件の賞賛
返信
0 返答(返信)