RX FIFO ERROR while both camera streaming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RX FIFO ERROR while both camera streaming

2,864件の閲覧回数
vimalan_93
Contributor I

Hi,

I am using the linux kernel 4.14.78 from sumo bsp in imx8m EVK (REV-B4) board. I can able to successfully stream the cameras in both minisas connectors individually. But when i tried to stream the both cameras simultaneously i received the RX_FIFO_OVERFLOW error. In NXP release notes they already mentioned about this issue i also attached the screenshot here for your referance. so, Is there any workaround for this issue.

When did you planned to deliver the next release?

Thanks

vimal.

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,727件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we do not have that type of information. I apologize for the inconveniences this could you.

Best regards,

Diego.

0 件の賞賛
返信

2,727件の閲覧回数
vimalan_93
Contributor I

Hi Diego Adrian Cuevas

I need to use both the cameras simultaneously, but when i tried to do the same i faced this RX_FIFO_OVERFLOW error from one of the camera very frequently. How to solve this issue? Any comments would really helpful for us.

Thanks,

Vimal.

0 件の賞賛
返信