RNDIS Support in imx6_kernel for Android 4.4.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RNDIS Support in imx6_kernel for Android 4.4.3

1,009 Views
bqam
Contributor I

when i connect usb to ethernet converter with otg USB of sabresd platform, it does not create any interface like usb0.

Where as when i check same converter with some other android board it shown interface usb0.

I am checking interface name using netcfg command.

also i have checked in kernel configuration to enable RNDIS mode but that option is not present in make menuconfig interface in imx6 kernel.

where as using beagle board kernel is supporting RNDIS mode and that option is enabled.

How do i add its driver in kernel.

Labels (3)
0 Kudos
Reply
0 Replies