RNDIS Support in imx6_kernel for Android 4.4.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RNDIS Support in imx6_kernel for Android 4.4.3

1,008件の閲覧回数
bqam
Contributor I

when i connect usb to ethernet converter with otg USB of sabresd platform, it does not create any interface like usb0.

Where as when i check same converter with some other android board it shown interface usb0.

I am checking interface name using netcfg command.

also i have checked in kernel configuration to enable RNDIS mode but that option is not present in make menuconfig interface in imx6 kernel.

where as using beagle board kernel is supporting RNDIS mode and that option is enabled.

How do i add its driver in kernel.

ラベル(3)
0 件の賞賛
返信
0 返答(返信)