RMII interface error on i.MX6Q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RMII interface error on i.MX6Q

跳至解决方案
11,754 次查看
laszlotimko
Contributor III

Hi everyone,

I have a custom hardware with i.MX6 Quad CPU. I would like to use its RMII interface to communicate with SMSC's LAN8720A PHY. Configuration, detection and communication seem to be right, but the problem is that all packets are received or transmitted by the PHY are totally wrong in fact. Below you can find an example ifconfig output, look at the statistics.

The connection is based on Freescale documentation: IMX6DQ6SDLHDG Rev 1 / Chapter 12.2. The part of schematic is attached. The system uses GPIO_16 pin to generate the reference clock. I measured the clock with frequency counter and is exact (<50ppm). The signal quality is a bit distorted, but is between LAN8720A's timing margins. I tried with different drive strengths, but none of them helped. An oscillogram is attached (in case of DSE=60Ohm). Anyway, I tried with external 50MHz clock on GPIO_16 with ENET_CLK_SEL:0, but same problem.

I observed the RMII lines with logic analyzer. It seems good to me, but I can't decode and interpret it.

RMII signals have 1410mils lengths, however REF_CLK has 1750mils.

I have already used LAN8720A with this connector successfully on another board, so physical part might not be the cause of error.

By the way, changing link's speed to 10Mbps does not help either.

Any help would be appreciated.

Best Regards,

     Laszlo Timko

Tested software versions:

U-Boot: imx_v2015.04_3.14.52_1.1.0_ga

Linux: 3.14.28_1.0.0_ga and imx_3.14.52_1.1.0_ga and imx_4.1.15_1.0.0_ga

Device tree:

&fec {

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_enet>;

        phy-mode = "rmii";

        phy-reset-gpios = <&gpio5 6 GPIO_ACTIVE_HIGH>;

        phy-reset-duration = <2>;

        status = "okay";

};

pinctrl_enet: enetgrp {

        fsl,pins = <

                MX6QDL_PAD_ENET_MDIO__ENET_MDIO         0x1b0a8

                MX6QDL_PAD_ENET_MDC__ENET_MDC           0x1b0a8

                MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0     0x1b0a8

                MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1     0x1b0a8

                MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN      0x1b0a8

                MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER       0x1b0a8

                MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0     0x1b0a8

                MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1     0x1b0a8

                MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN       0x1b0a8

                MX6QDL_PAD_GPIO_16__ENET_REF_CLK        0x4001b0a1

                MX6QDL_PAD_DISP0_DAT12__GPIO5_IO06      0x1b0b0 /* ENET_RST */

                MX6QDL_PAD_DISP0_DAT11__GPIO5_IO05      0x1b0b0 /* ENET_INT */

        >;

};

The changes made in kernel source to generate 50MHz clock:

linux-2.6-imx-rel_imx_3.14.28_1.0.0_ga/arch/arm/mach-imx/clk-imx6q.c:

@@ -568,8 +568,8 @@

                imx_clk_prepare_enable(clk[IMX6QDL_CLK_USBPHY2_GATE]);

        }

-       /*Set enet_ref clock to 125M to supply for RGMII tx_clk */

-       clk_set_rate(clk[IMX6QDL_CLK_ENET_REF], 125000000);

+       /*Set enet_ref clock to 50M to supply for RMII tx_clk */

+       clk_set_rate(clk[IMX6QDL_CLK_ENET_REF], 50000000);

#ifdef CONFIG_MX6_VPU_352M

        /*

Register values verification:

IOMUXC_SW_PAD_CTL_PAD_GPIO16:

        root@mx6obu:~# devmem2 0x20e0618 w

        Value at address 0x20E0618 (0x76f90618): 0x1B0A1 (-> 60Ohm DSE, SRE)

IOMUXC_SW_MUX_CTL_PAD_GPIO16:

        root@mx6obu:~# devmem2 0x20e0248 w

        Value at address 0x20E0248 (0x76fc0248): 0x12 (-> SION, ALT2:ENET_REF_CLK)

IOMUX_ENET_REF_CLK_SELECT_INPUT:

        root@mx6obu:~# devmem2 0x20e083C w

        Value at address 0x20E083C (0x76f1983c): 0x1 (-> DAISY - GPIO16_ALT2)

IOMUXC_GPR1:

        root@mx6obu:~# devmem2 0x20e0004

        Value at address 0x20E0004 (0x76fdb004): 0x48693005 (-> ENET_CLK_SEL:1)

PHY related kernel boot log:

[    1.260400] libphy: fec_enet_mii_bus: probed

[    1.263863] fec 2188000.ethernet eth0: registered PHC device 0

[   15.536851] fec 2188000.ethernet eth0: Freescale FEC PHY driver [SMSC LAN8710/LAN8720] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)

[   15.548649] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready

[   19.696915] libphy: 2188000.ethernet:01 - Link is Up - 100/Full

[   19.701573] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready

Ethernet info:

root@mx6obu:~# ethtool eth0

Settings for eth0:

        Supported ports: [ TP MII ]

        Supported link modes:   10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Supported pause frame use: Symmetric

        Supports auto-negotiation: Yes

        Advertised link modes:  10baseT/Half 10baseT/Full

                                100baseT/Half 100baseT/Full

        Advertised pause frame use: Symmetric

        Advertised auto-negotiation: Yes

        Link partner advertised link modes:  10baseT/Half 10baseT/Full

                                             100baseT/Half 100baseT/Full

        Link partner advertised pause frame use: No

        Link partner advertised auto-negotiation: Yes

        Speed: 100Mb/s

        Duplex: Full

        Port: MII

        PHYAD: 1

        Transceiver: external

        Auto-negotiation: on

        Supports Wake-on: d

        Wake-on: d

        Link detected: yes

root@mx6obu:~# ifconfig eth0

eth0      Link encap:Ethernet  HWaddr 00:40:95:36:35:33 

          inet addr:10.0.3.174  Bcast:10.0.3.255  Mask:255.255.252.0

          inet6 addr: fe80::240:95ff:fe36:3533/64 Scope:Link

          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1

          RX packets:98 errors:98 dropped:26 overruns:0 frame:98

          TX packets:76 errors:0 dropped:0 overruns:0 carrier:0

          collisions:0 txqueuelen:1000

          RX bytes:28847 (28.1 KiB)  TX bytes:6949 (6.7 KiB)

U-Boot log:

Net:   eth_init: fec_probe(bd, -1, 1) @ 02188000

fec_mii_setspeed: mii_speed 0000001a

fec_mdio_read: phy: 01 reg:02 val:0x7

fec_mdio_read: phy: 01 reg:03 val:0xc0f1

fec_mii_setspeed: mii_speed 0000001a

fec_mdio_read: phy: 01 reg:00 val:0x3000

fec_mdio_write: phy: 01 reg:00 val:0xb000

fec_mdio_read: phy: 01 reg:00 val:0x3000

FEC connected to SMSC LAN8710/LAN8720

fec_mdio_read: phy: 01 reg:04 val:0x1e1

fec_mdio_read: phy: 01 reg:00 val:0x3000

FEC [PRIME]

=> ping 10.0.0.102

eth_halt: wait for stop regs

eth_halt: done

fec_mii_setspeed: mii_speed 0000001a

fec_open: fec_open(dev)

fec_mdio_read: phy: 01 reg:01 val:0x782d

fec_mdio_read: phy: 01 reg:01 val:0x782d

fec_mdio_read: phy: 01 reg:04 val:0x1e1

fec_mdio_read: phy: 01 reg:05 val:0x41e1

fec_open:Speed=100

Using FEC device

fec_send: status 0xc00 index 0 ret 0

fec_recv: ievent 0xc000000

fec_recv: status 0x8000

fec_recv: stop

fec_recv: ievent 0x0

fec_recv: status 0x8000

fec_recv: stop

fec_recv: ievent 0x0

fec_recv: status 0x8000

fec_recv: stop

fec_recv: ievent 0x0

fec_recv: status 0x8000

ARP Retry count exceeded; starting again

ARP Retry count exceeded; starting again

...

Part of schematic:

phy_conn.png

REF_CLK scope measurement:

default_dse110.png

Analyzer output sample (RMII_TXD):

analyzer_txd.png

标签 (2)
1 解答
5,750 次查看
laszlotimko
Contributor III

Finally, I have found the solution.

As can be seen in schematic, ENET_RXD0 is connected to RMII_RXD1, ENET_RXD1 to RMII_RXD0, ENET_TXD0 to RMII_TXD1 and ENET_TXD1 to RMII_TXD0. Ethernet instantly started to work when I fixed these lines.

Thank everyone for the help!

在原帖中查看解决方案

7 回复数
5,751 次查看
laszlotimko
Contributor III

Finally, I have found the solution.

As can be seen in schematic, ENET_RXD0 is connected to RMII_RXD1, ENET_RXD1 to RMII_RXD0, ENET_TXD0 to RMII_TXD1 and ENET_TXD1 to RMII_TXD0. Ethernet instantly started to work when I fixed these lines.

Thank everyone for the help!

5,750 次查看
laszlotimko
Contributor III

I am still struggling with this problem and I am starting to run out of ideas. Is anyone using combination of i.MX6 Dual or Quad CPU with LAN8720 PHY and 3.14 or newer kernel successfully?

0 项奖励
回复
5,750 次查看
wei-fonglin
Contributor II

Hi Laszlo Timko,

I have the same problem.

After I mark below line in file:arch/arm/mach-imx/clk-imx6q.c function:imx6q_clocks_init, it fix this problem.

clk_set_rate(clk[enet_ref], 125000000);

Hope it is useful for you.

Best Regards,

Frank

0 项奖励
回复
5,750 次查看
Sasamy
Contributor IV

Hi Laszlo Timko,

MX6QDL_PAD_GPIO_16__ENET_REF_CLK        0x1b0a1

...

IOMUXC_SW_MUX_CTL_PAD_GPIO16:

        root@mx6obu:~# devmem2 0x20e0248 w

        Value at address 0x20E0248 (0x76fc0248): 0x12 (-> SION, ALT2 - ENET_REF_CLK)

as far as I can see SION is not enabled in the gpio16 configuration, we use LAN8720A on SOLO and DUAL and in our case pin configured as here

MX6QDL_PAD_GPIO_16__ENET_REF_CLK        0x4001b0a8

Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt

SION(1 << 30): Software Input On Field.

Force the selected mux mode input path no matter of MUX_MODE functionality.

Alexander

0 项奖励
回复
5,750 次查看
laszlotimko
Contributor III

Dear Alexander,

Thank you so much for your advice.

However, as I see it, SION bit is indeed enabled:

  0x12 -> 10010 -> 5th bit is 1

It has been activated in arch/arm/boot/dts/imx6q-pinfunc.h:

  -#define MX6QDL_PAD_GPIO_16__ENET_REF_CLK            0x248 0x618 0x83c 0x2 0x1

  +#define MX6QDL_PAD_GPIO_16__ENET_REF_CLK            0x248 0x618 0x83c 0x12 0x1

Anyway, I have tested with 0x4001b0a8 value too and did not help.

Regards,

  Laszlo

0 项奖励
回复
5,750 次查看
Yuri
NXP Employee
NXP Employee

   Please check Your configuration regarding recommendations in Chapter 9

(Porting the Ethernet Controller Driver) of "i.MX_6_BSP_Porting_Guide.pdf"

in Linux documentation.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
5,750 次查看
laszlotimko
Contributor III

Dear Yuri,

Thanks for your reply, I didn't know documentation like this existed. That would certainly aid in the future, but it did not help to solve my ethernet problem.

It would be helpful to rule out software error, if someone confirmed that RMII interface actually works with 3.14 kernel.

Sincerely

0 项奖励
回复