Changing IPU Parameters via Gstreamer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changing IPU Parameters via Gstreamer

Jump to solution
1,835 Views
jeromehaxhiaj
Contributor I

Hi everyone,

I'm playing a video with gstreamer on an IMX6 Quad. Is it possible with gstreamer to  select the component which make the CSC ( IC or DP ) ?

Thanks

Labels (4)
1 Solution
1,652 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jerome

as mentioned on below links option with IC is only available

https://community.freescale.com/thread/308426

https://community.freescale.com/docs/DOC-94961

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,653 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jerome

as mentioned on below links option with IC is only available

https://community.freescale.com/thread/308426

https://community.freescale.com/docs/DOC-94961

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------