RGMII and RMII interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RGMII and RMII interface

9,235件の閲覧回数
riteshpatel
Contributor II

Hi,

We have used iMX6Q processor (DART-MX6 Variscite SOM) in my design. We have connected iMX6Q RGMII interface with RMII interface of KSZ8081 PHY. Find attached schematic. 

Ethernet interface is not working on our hardware.

Please review & let us know what modifications are required to work RGMII interface as a RMII on iMX6Q processor.

Seeking for your early response.

Thanks,

Ritesh

ラベル(2)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

7,608件の閲覧回数
riteshpatel
Contributor II

Hi

Any update??

0 件の賞賛
返信

7,608件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Ritesh,

    please remove R47, and populate R50!

    It means we will use RMII_REF_CLK to be PHY's working clock and MAC reference clock!

Then try!

Hope above suggestion can help you!

Best Regards,

Weidong

0 件の賞賛
返信

7,608件の閲覧回数
riteshpatel
Contributor II

Hi Weiding,

To clarify further, I have connected RGMII interface of iMX6Q with KSZ8081 which only support RMII interface.

Thanks

0 件の賞賛
返信

7,608件の閲覧回数
riteshpatel
Contributor II

Hi Weiding,

Thanks for quick response.

Can you let us know which modifications required in firmware/driver to convert RGMII to RMII interface? I have connected RGMII interface of iMX6Q to RMII interface of KSZ8081 PHY.

Thanks.

0 件の賞賛
返信

5,715件の閲覧回数
fx73
Contributor I

"Can you let us know which modifications required in firmware/driver to convert RGMII to RMII interface?"

Did you ever find out what software mods were required to get the RMII to function?

0 件の賞賛
返信

7,173件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

RGMII and RMII use different pins. You can find the RMII pin list in the reference manual. If you use RGMII pins, this cannot be modified in software.

 

weidong

0 件の賞賛
返信

7,265件の閲覧回数
2548903578
Contributor III

Hi,

Is your problem solved? Now I also use this chip, and the interface is also converted from RGMII to RMII

0 件の賞賛
返信