RGMII ENET_REF_CLK input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RGMII ENET_REF_CLK input

ソリューションへジャンプ
2,587件の閲覧回数
frankambrosius
Contributor II

We will connect a 125MHz external clock to the ENET_REF_CLK pad.

Does this clock have to be up and running before or after we power-up the i.MX6?

Best regards,

Frank

ラベル(1)
0 件の賞賛
返信
1 解決策
2,315件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Frank

clock can be provided at any time after power-up sequence.

~igor

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,314件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Frank

clock should be provided to i.MX after its power-up, in general

it is not allowed to provide signals to unpowered processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,314件の閲覧回数
frankambrosius
Contributor II

Hi Igor,

Thanks for the answer.

Are there any restrictions on before what moment the clock should be up.

Of course it has to be up before actual RGMII communication can start. Is it a problem if it comes up while or after initializing the RGMII interface (while booting the imx)?

Best regards,

Frank

0 件の賞賛
返信
2,316件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Frank

clock can be provided at any time after power-up sequence.

~igor

0 件の賞賛
返信