RGMII ENET_REF_CLK input

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RGMII ENET_REF_CLK input

Jump to solution
2,579 Views
frankambrosius
Contributor II

We will connect a 125MHz external clock to the ENET_REF_CLK pad.

Does this clock have to be up and running before or after we power-up the i.MX6?

Best regards,

Frank

Labels (1)
0 Kudos
Reply
1 Solution
2,307 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frank

clock can be provided at any time after power-up sequence.

~igor

View solution in original post

0 Kudos
Reply
3 Replies
2,306 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frank

clock should be provided to i.MX after its power-up, in general

it is not allowed to provide signals to unpowered processor.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

2,306 Views
frankambrosius
Contributor II

Hi Igor,

Thanks for the answer.

Are there any restrictions on before what moment the clock should be up.

Of course it has to be up before actual RGMII communication can start. Is it a problem if it comes up while or after initializing the RGMII interface (while booting the imx)?

Best regards,

Frank

0 Kudos
Reply
2,308 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frank

clock can be provided at any time after power-up sequence.

~igor

0 Kudos
Reply