RE: Yocto Build procedure and Kernal Device tree configuration.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RE: Yocto Build procedure and Kernal Device tree configuration.

1,100件の閲覧回数
subbuemdtest
Contributor I

Hi @nxp,

 

We want to create Custom Yocto Build image and Device Tree Configuration for ARM 8MPLUSLPD4-EVK (IMX8MPLUS ). So please provide the steps for Building the yocto image and Kernel Device tree configuration to enable the drivers. Waiting for your valuable response.


Thanks,

Subbu.
 

 

 

 

Thanks,

 

Subbu.

0 件の賞賛
返信
3 返答(返信)

1,085件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

HI @subbuemdtest!
Thank you for contacting NXP Support!

 

To create the image using Yocto you can refer to our YOCTO PROJECT USERS GUIDE.

After that you have two options:

Configure the Kernel source using devshell 

Creating and applying a git patch in a yocto build 

 

Also you can consult all our documentation in our web page. 

 

Best Regards!

Chavira

0 件の賞賛
返信

1,074件の閲覧回数
subbuemdtest
Contributor I
Hi @Chariva,

Thanks for response. I want inputs from you regarding LVDS-HDMI channel enable in my yocto image. And I want know the what are all the dts files into change for enabling the LVDS-HDMI Driver. And what are all the dtb files need to include Boot file system.

Thanks
Subbu
0 件の賞賛
返信

1,067件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @subbuemdtest!

imx8mp-evk.dtb: Supports single or multiple displays with HDMI, MIPI-DSI-HDMI, and
LVDS-HDMI

 

You can consult the different device tree and their functionalities in our Linux Release Notes 

0 件の賞賛
返信