RAM FLASH combine pakage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM FLASH combine pakage

1,337件の閲覧回数
aieenrezai
Contributor I

Dear sir/Madam,

We want to used combine package of ram and nand flash such as:

MT29TZZZ8D5JKETS-107 W.95Q

or

MT29TZZZ8D5JKEZB-107 W.95Q

however they are not listed as supported device in NXP micron compatible list

https://www.micron.com/~/media/documents/products/other-documents/nxp_compatibility_chart.pdf 

is using these devices straight forward?

or I have to change parameters in the processor? how I have to change them?

our processor is IMX7D

Bests

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,258件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi aieen

unfortunately datasheets for these parts are not publicly available,

if you have them, one can send them using service request for evaluating parts for usage.

https://community.nxp.com/docs/DOC-329745 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信