Question, i.MX6Quad power-on sequence

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question, i.MX6Quad power-on sequence

跳至解决方案
1,155 次查看
SLICE
Contributor IV

Dear team,

I would like to ask about power-on sequence for i.MX6Q.

After reading chapter 4 in your Hardware Development Guide for i.MX6Quad, my customer wants to know whether the following sequence, in the following order, can be allowed.

-  2.8V(VDDHIGH_IN) and 1.2V(NVCC_RGMII) are turned on simultaneously.

-  Then, 3.3V(NVCC_EIM0~2,NVCC_ENET,NVCC_GPIO,NVCC_SD3,NVCC_NANDF,NVCC_JTAG) and 2.5V(NVCC_CSI,NVCC_SD1,NVCC_SD2) are turned on simultaneously.

-  Then, NVCC_DRAM(1.5V) is turned on.

 

Could you show me whether the above is allowed?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 解答
1,025 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes such power-up sequence is allowed, note VDD_SNVS_IN supply must be

turned on before any other power supply and it may be connected (shorted) with VDD_HIGH_IN supply.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,026 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes such power-up sequence is allowed, note VDD_SNVS_IN supply must be

turned on before any other power supply and it may be connected (shorted) with VDD_HIGH_IN supply.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复