imx6sl, YOCTO-Upgradation:: 3.10.17 to 3.14

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6sl, YOCTO-Upgradation:: 3.10.17 to 3.14

312 Views
ashishsbn
Contributor I

Hi,

I am working on imx6sl board and Yocto Linux SDK.
currently i have yocto Linux kernel 3.10.17 by default on it, I need to upgrade it to version 3.14.
Can someone guide me with the steps required for the same.


Thanks
Ashish S

Labels (4)
0 Kudos
1 Reply

258 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ashish

please follow Yocto User Guide included in Linux 3.14.52 Doc package

http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos