Question, i.MX6Q PCIe refClk usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6Q PCIe refClk usage

1,515 Views
Aemj
Contributor IV

Dear team,

I would like to ask about PCIe reference clock of i.MX6Q.

In your latest i.MX6DQ Hardware development guide(IMX6DQ6SDLHDG, Rev.2.), it is stated as below in Table 2-10 ‘PCIe recommendations’.

“1. An external PCIe reference clock generator is recommended. i.MX differential clock is not compliant with PCIe standard.

i.MX differential clock does not meet PCIe compliance standards”

Now my customer is using the PCIe interface on their board, and CLK1_N/P from i.MX6 are used for external FPGA as a reference clock.

After reading the latest HDG, they have a concern on the PCIe refClock use.

Should they change their current design into using an external ref clock?

 

Thanks,

Miyamoto

Labels (2)
0 Kudos
Reply
1 Reply

1,149 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

>Should they change their current design into using an external ref clock?

yes, more details are provided on

PCIe REFCLK 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply