(Q3) Required queries about IMX6 ultra lite processor and its Errata. Need help for clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

(Q3) Required queries about IMX6 ultra lite processor and its Errata. Need help for clarification

950 Views
ramesh6663
Contributor III

Reset circuitry in IMX6UL reference design query:


The below shows the NXP reference design reset circuits. NXP ref design used two different reset circuits for i.MX6UL & PMIC.

Q4.png

1.Why do we require two different reset circuit? Could you please explain?


2.We followed simple reset circuit to PMIC power on pin as shown figure below, this circuit was taken from our existing i.MX6 Solo design which was already working, we hope it will work same for PMIC PF3001 part as well. Am i right?

Q5.png

3.  Is there any silicon version issue for new version (i.MX6UL)?

Thanks in advance

Thanks & Regards,

Ramesh

Labels (1)
0 Kudos
Reply
1 Reply

875 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramesh

1. please refer to

https://community.nxp.com/message/862062?commentID=862062#comment-862062 

2. I think it should work fine with PMIC PF3001 as well

3. no

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply