Question, NAND Flash for i.MX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, NAND Flash for i.MX25

Jump to solution
4,010 Views
Aemj
Contributor IV

Dear team,

I would like to ask about NAND flash chip which can use for i.MX25.

My customer wants to know if they can use TC58NVG0S3HTAI0B4H NAND Flash chip for i.MX25.

Actually, they are using TC58NVM9S3ETAI0 with i.MX25 for their current product.

Due to EOL of the current NAND Chip, they have to change the NAND chip.

Could you show me whether TC58NVG0S3HTAI0B4H can be used for i.MX25?

Their concerns are;

The spec of ECC and the size of redundancy area.

Please find the attached file for TC58NVG0S3HTAI0B4H.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
3,806 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Looks like this was already discussed in

Question, i.MX25 NAND boot 

https://community.nxp.com/message/598383 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
3,806 Views
Aemj
Contributor IV

Thanks, I remember now.

Miyamoto

0 Kudos
Reply
3,807 Views
Yuri
NXP Employee
NXP Employee

Hello,

   Looks like this was already discussed in

Question, i.MX25 NAND boot 

https://community.nxp.com/message/598383 

Regards,

Yuri.

0 Kudos
Reply