Question, NAND chip TC58NVG0S3 use for i.MX25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, NAND chip TC58NVG0S3 use for i.MX25

2,127 Views
Aemj
Contributor IV

Dear team,

A while ago, we received the answer on Toshiba/TC58NVG0S3 NAND chip use for i.MX25 from this community as below.

https://community.freescale.com/thread/379638

And it says that Toshiba/TC58NVG0S3 NAND flash chip cannot meet the specification of i.MX25 NFC.

We found the description table entry of “TC58NVG0S3” in your LinuxBSP, L2.6.31_09.12.00, source code.

It is written in nand_device_info_table_type_2[] structure in drivers/mtd/nand/nand_device_info.c file in the LinuxBSP.

If the code has not been tested, I mean whether the table entry of TC58NVG0S3 can really work is not sure,

Then Can I understand the NAND chip might be used as NAND device under the Linux but the NAND chip still cannot be used for Boot device?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
3 Replies

1,907 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The main restriction for TC58NVG0S3 with i.MX25 NFC relates to possible reliability

issues, since when considering NAND datasheet (in the Community thread) I found

information about page = (2K + 128) bytes and 8-bit ECC ; but the i.MX25 NFC uses

for such NANDs 4-bit ECC. 
Nevertheless, today I found the TC58NVG0S3 Datasheet, where there is no such
statement about 8-bit ECC. So, please consult with the manufacturer if TC58NVG0S3
page organization of (2K + 128) can be reliably used with 4-bit ECC. If so – yes we
can use this NAND with i.MX25.  


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,907 Views
Aemj
Contributor IV

Hi Yuri,

Thanks for your comment.

Could you show me the boot-pin settings for supporting page=(2K + 128) bytes NAND?

Or can I understand such NAND which has a page-size of (2K+128)bytes still cannot be used for boot?

Thanks,

Miyamoto

0 Kudos
Reply

1,907 Views
Yuri
NXP Employee
NXP Employee

Hello,

* BT_PAGE_SIZE[1:0]  = 01 (2K)

* BT_BUS_WIDTH =  00 (8-bit)

* BT_SPARE_SIZE = 0  (128 bytes)

* BT_MEM_TYPE[1:0] = 01  (4 address cycles)

* BT_MLC_SEL - you may try both SLC or MLC

Regards,

Yuri.

0 Kudos
Reply