Question, NAND Flash for i.MX25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, NAND Flash for i.MX25

ソリューションへジャンプ
3,870件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about NAND flash chip which can use for i.MX25.

My customer wants to know if they can use TC58NVG0S3HTAI0B4H NAND Flash chip for i.MX25.

Actually, they are using TC58NVM9S3ETAI0 with i.MX25 for their current product.

Due to EOL of the current NAND Chip, they have to change the NAND chip.

Could you show me whether TC58NVG0S3HTAI0B4H can be used for i.MX25?

Their concerns are;

The spec of ECC and the size of redundancy area.

Please find the attached file for TC58NVG0S3HTAI0B4H.

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
3,666件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Looks like this was already discussed in

Question, i.MX25 NAND boot 

https://community.nxp.com/message/598383 

Regards,

Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,666件の閲覧回数
Aemj
Contributor IV

Thanks, I remember now.

Miyamoto

0 件の賞賛
返信
3,667件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Looks like this was already discussed in

Question, i.MX25 NAND boot 

https://community.nxp.com/message/598383 

Regards,

Yuri.

0 件の賞賛
返信