QT Application launching issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QT Application launching issue

16,661件の閲覧回数
lavakumars
Contributor IV

hi,

I am working on imx6qp sabre AI board. with kernel version: 4.1.15 . image freescale image built with "xwayland" setup

earlier image was built with qt (meta-qt5) version :5.5 and the application compiled with that toolchain was successfully launched .

but now I changed the meta-qt5 layer to 5.7 master branch. but the application built with its toolchain is not launching but throwing some errors like : cannot find EGLCONFIG returning null config.

                           QwaylandGlcontext : failed to create EGLcontext error:3905. etc

can someone help me to solve this?

Please also check the attachments for the error logs.

Adding some more images for extra input. used the qt examples to build and run (able to build successfully but failed to execute )

Regards,

Lavakumar S

0 件の賞賛
返信
7 返答(返信)

15,662件の閲覧回数
xinyu_chen
NXP Employee
NXP Employee

You properly need qtwayland plugin, and a compositor like weston. Please check your package.

0 件の賞賛
返信

15,662件の閲覧回数
lavakumars
Contributor IV

hi Eric Chen,

Thanx, I have wayland, Weston installed and running.

qtwayland also built all together with meta-qt5.

: But as I can see there is no eglfs platform plugins. is that a issue..?can you help on that?

Regards

Lavakumar s

0 件の賞賛
返信

15,662件の閲覧回数
xinyu_chen
NXP Employee
NXP Employee

Hi Lavakumar

The EGLFS should be default backend of the wayland compositor. Please check your yocto bb file for weston.

Also compare this to the 5.6.

0 件の賞賛
返信

15,662件の閲覧回数
lavakumars
Contributor IV

hi Maxim Kuk,

can you help me here. i saw you worked on qt 5.7.0(here). i am facing some issues with application launching (hmi).

issues with qtwayland. actually my image built xwayland DISTRO.

Eric Chen : can you help here?.

Regards,

Lavakumar S

0 件の賞賛
返信

15,662件の閲覧回数
maximkuk
Contributor III

Sorry, but I don't work with wayland.
Maybe it is wayland issue itself? Or maybe you use old yocto version?

When I updated Qt to 5.7 I also updated yocto from 1.8 to 2.1.2

0 件の賞賛
返信

15,662件の閲覧回数
b36401
NXP Employee
NXP Employee

Please apply patches noted in this message:
https://community.nxp.com/message/489133?commentID=489133#comment-450084

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

15,662件の閲覧回数
lavakumars
Contributor IV

hi Victor Linnik,

Thanks for the reply..

Applied the above patches but no use...

when I revert back the meta-qt5 to version 5.5 the built application works fine. gives above errors and doesn't work if I revert meta-qt5 layer to v5.7 :smileysad:.

Regards,

Lavakumar S

0 件の賞賛
返信