QSPI for IMX8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSPI for IMX8M Plus

Jump to solution
1,845 Views
waynechung2
Contributor III

Hi,

Could we use the QSPI for IMX8M Plus M7 ?

If it work, where can i find the driver ?

Thanks.

Best Regards,

Wayne.

0 Kudos
Reply
1 Solution
1,840 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

If you mean that if it is possible that the binary file runs at QSPI/XIP, then yes it is possible, please refer to the getting started with MCUXpresso SDK for EVK-MIMX8MP.

If you mean that M7 has access to the QSPI, then no, usually this peripheral is assigned to the Cortex-A, so we do not provide a driver for cortex-M.

Best regards,
Aldo.

View solution in original post

0 Kudos
Reply
1 Reply
1,841 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

If you mean that if it is possible that the binary file runs at QSPI/XIP, then yes it is possible, please refer to the getting started with MCUXpresso SDK for EVK-MIMX8MP.

If you mean that M7 has access to the QSPI, then no, usually this peripheral is assigned to the Cortex-A, so we do not provide a driver for cortex-M.

Best regards,
Aldo.

0 Kudos
Reply