Q: IPU + image scrolling [Linux]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Q: IPU + image scrolling [Linux]

1,618 Views
maxx
Contributor I

Hello!

I need to implement image scrolling under Linux on a imx535.

According to the " i.MX53 Multimedia Applications Processor Reference Manual", 45.3.1.6.2 Update Of The Display Buffer:

"Automatic display of a changing image (animation) or moving image (scrolling) This

is implemented by reading frames (from a full plane buffer) with incremental offset"

Seems that is exactly what I need. I tried to research IPU driver located in $BUILD/linux/drivers/mxc/ipu*, but seems that current implementation of IPU driver and therefore user-space library does not support scrolling feature at all.

Does anybody dig into this field yet? I also tried to search IMX community - no results so far:(


Thanks for any info!

Labels (2)
0 Kudos
Reply
1 Reply

1,226 Views
jimmychan
NXP TechSupport
NXP TechSupport

Unfortunately, there is no example for the moving image (scrolling). For details, please read the i.MX53RM Chapter 45.5.2.7.1 Scrolling support and 45.5.2.10 CPMEM - Channel Parameter Memory.  You may need set the values in cpmem and implement it by yourself.

0 Kudos
Reply