Hello all!
Thanks to all who helped me in getting started with imx28 evk. I have properly booted up the board and test the eth0 as well but there is a problem in eth0
1. How can I permanently store the setting i.e. ip address assigned because I have to assign the IP address every time I start up
2. The eth0 works properly when I first set it to up. but if I set it to down and then want to up it it gives the following error
PHY can not be attached
device or resource busy
How can I fix these 2 problems???
解決済! 解決策の投稿を見る。
http://www.kernel.org/doc/Documentation/kernel-parameters.txt
You can pass kernel parameter in form of:
ip=<client-ip>:<server-ip>:<gw-ip>:<netmask>:<hostname>:<device>:<autoconf>
So it could be as simple as:
ip=192.168.0.1
or
ip=dhcp
Or you could run ifconfig as part of your startup scripts etc...
http://www.kernel.org/doc/Documentation/kernel-parameters.txt
You can pass kernel parameter in form of:
ip=<client-ip>:<server-ip>:<gw-ip>:<netmask>:<hostname>:<device>:<autoconf>
So it could be as simple as:
ip=192.168.0.1
or
ip=dhcp
Or you could run ifconfig as part of your startup scripts etc...