Proper details required to execute and check Flash-loader SDK example code

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Proper details required to execute and check Flash-loader SDK example code

473 次查看
darshanmk
Contributor I

Hi,

I'm using i.MXRT1170-evkb board. I am trying to run the NXP provided Flash-loader SDK example code for CM7 core. I couldn't find any Readme.md file. So if I want to analyze the code provided in the example I'm facing difficulty to understand for what purpose this example has been provided.

And I want to know which Flash memory is being used in the same example. I have attached the MEMORY section in linker script, there I couldn't understand which memory section is being used.

darshanmk_0-1735821945919.png

Please help me regarding this.

0 项奖励
回复
1 回复

451 次查看
mayliu1
NXP Employee
NXP Employee

Hi @darshanmk 

Thank you so much for your interest in our products and for using our community.

mayliu1_0-1735888293112.png

When you import this SDK demo, it will show some introduction  about this demo.  The  flashloader is a bootloader that executes from target RAM memory on the platform.

what you upload memory picture address  is OCRAM address.

mayliu1_1-1735888611046.png

For more information I suggest you can  refer to these Link:

1: https://www.nxp.com/docs/en/nxp/application-notes/AN12238.pdf

2: Bootloader Code - NXP Community

Wish it helps you.

BR

mayliu

0 项奖励
回复