Problems with DDR setup on i.MX6D

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Problems with DDR setup on i.MX6D

跳至解决方案
2,037 次查看
christiangmeine
Contributor I

I am currently working on board bring-up for our custom design based on the i.MX6D.

I have tried the i.Mx6DQSDL DDR3 Script Aid [1] and got mixed results. It is needed to

select the ARM core speed. Does this mean I need to run the semi-automatic calibration

process for every ARM core speed I want to support? u-boot start with ~800 MHz but

later on the linux kernel could change the ARM core speed up to 1.2 GHz.

[1] https://community.freescale.com/docs/DOC-94917

标签 (3)
0 项奖励
回复
1 解答
1,705 次查看
VladanJovanovic
NXP Employee
NXP Employee

No, calibration is not needed to be run when you change ARM core speed. What kind of mixed results do you get?

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,705 次查看
YixingKong
Senior Contributor IV

Chris, if your question has been answered, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 项奖励
回复
1,706 次查看
VladanJovanovic
NXP Employee
NXP Employee

No, calibration is not needed to be run when you change ARM core speed. What kind of mixed results do you get?

0 项奖励
回复
1,705 次查看
christiangmeine
Contributor I

That is good to know. It turned out that we had some problems with our first prototype. All of them

seem to be fixed and our custom board runs quite well.

I am quite sorry the noise.

0 项奖励
回复