Problems with DDR setup on i.MX6D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with DDR setup on i.MX6D

ソリューションへジャンプ
2,086件の閲覧回数
christiangmeine
Contributor I

I am currently working on board bring-up for our custom design based on the i.MX6D.

I have tried the i.Mx6DQSDL DDR3 Script Aid [1] and got mixed results. It is needed to

select the ARM core speed. Does this mean I need to run the semi-automatic calibration

process for every ARM core speed I want to support? u-boot start with ~800 MHz but

later on the linux kernel could change the ARM core speed up to 1.2 GHz.

[1] https://community.freescale.com/docs/DOC-94917

ラベル(3)
0 件の賞賛
返信
1 解決策
1,754件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

No, calibration is not needed to be run when you change ARM core speed. What kind of mixed results do you get?

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,754件の閲覧回数
YixingKong
Senior Contributor IV

Chris, if your question has been answered, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 件の賞賛
返信
1,755件の閲覧回数
VladanJovanovic
NXP Employee
NXP Employee

No, calibration is not needed to be run when you change ARM core speed. What kind of mixed results do you get?

0 件の賞賛
返信
1,754件の閲覧回数
christiangmeine
Contributor I

That is good to know. It turned out that we had some problems with our first prototype. All of them

seem to be fixed and our custom board runs quite well.

I am quite sorry the noise.

0 件の賞賛
返信