Problems with DDR setup on i.MX6D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with DDR setup on i.MX6D

Jump to solution
2,812 Views
christiangmeine
Contributor I

I am currently working on board bring-up for our custom design based on the i.MX6D.

I have tried the i.Mx6DQSDL DDR3 Script Aid [1] and got mixed results. It is needed to

select the ARM core speed. Does this mean I need to run the semi-automatic calibration

process for every ARM core speed I want to support? u-boot start with ~800 MHz but

later on the linux kernel could change the ARM core speed up to 1.2 GHz.

[1] https://community.freescale.com/docs/DOC-94917

Labels (3)
0 Kudos
Reply
1 Solution
2,480 Views
VladanJovanovic
NXP Employee
NXP Employee

No, calibration is not needed to be run when you change ARM core speed. What kind of mixed results do you get?

View solution in original post

0 Kudos
Reply
3 Replies
2,480 Views
YixingKong
Senior Contributor IV

Chris, if your question has been answered, please click Correct Answer/Helpful Answer.

Thanks,

Yixing

0 Kudos
Reply
2,481 Views
VladanJovanovic
NXP Employee
NXP Employee

No, calibration is not needed to be run when you change ARM core speed. What kind of mixed results do you get?

0 Kudos
Reply
2,480 Views
christiangmeine
Contributor I

That is good to know. It turned out that we had some problems with our first prototype. All of them

seem to be fixed and our custom board runs quite well.

I am quite sorry the noise.

0 Kudos
Reply