Price vs Performance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Price vs Performance

Jump to solution
3,128 Views
salihsonmez
Contributor I

I notice that IMX6 serisi is cheapper than processor with powerpc cores. for example IMX6Dual core is cheaper than P2020. When I compare both as performance ,  P2020 is not extremely powerful as compare with IMX6 dual core. Is there any reason  that I don't notice?

0 Kudos
Reply
1 Solution
2,910 Views
Yuri
NXP Employee
NXP Employee

The QorIQ processors are intended for specific (network) applications,

with (relatively) strong technical requirements (environment, reliability, etc)

and (relatively) restricted market.

The i.MX6 (mainly) are intended for general multimedia (mass market)

applications.

View solution in original post

0 Kudos
Reply
4 Replies
2,910 Views
salihsonmez
Contributor I

So , Am I correct, the reason of their price differences are not performance values (Integer and floating point operations). ? It is ımportant for me that I dont  want to ignore or pass over any important performance difference between two processor?

0 Kudos
Reply
2,910 Views
Yuri
NXP Employee
NXP Employee

For network related operations QorIQ performance may significantly exceed i.MX6 one (even for the same Ethernet speed).

0 Kudos
Reply
2,910 Views
salihsonmez
Contributor I

Thanks for quick answer.

0 Kudos
Reply
2,911 Views
Yuri
NXP Employee
NXP Employee

The QorIQ processors are intended for specific (network) applications,

with (relatively) strong technical requirements (environment, reliability, etc)

and (relatively) restricted market.

The i.MX6 (mainly) are intended for general multimedia (mass market)

applications.

0 Kudos
Reply