Hi,
Any input on above qestions?
Hello,John,
What OS are you using ? linux or anddroid released by freesclae ? or other RTOS ?
If you are using freescale's BSP, you only need IOMUX I2S signal via AUD6 port .
Regards,
Weidong
I am using android 13.4.1 released by freescale only. Thanks for your replay.
Hello,John,
Please refer to the following steps:
(1)iomux to PADs(See Reference manual)
AUD6_TXC--->DI0_PIN15
AUD6_TXFS---->DI0_PIN3
AUD6_TXD----->DI0_PIN2
AUD6_RXD----->DI0_PIN4
(2)add them to iomux structure
Open file liunx/arch/arm/mach-mx6/board-mx6q_sabresd.h
static iomux_v3_cfg_t mx6q_sabresd_pads[] = {
/* AUDMUX por 6 */
MX6Q_PAD_DI0_PIN15__AUDMUX_AUD6_TXC,
MX6Q_PAD_DI0_PIN3__AUDMUX_AUD6_TXFS,
MX6Q_PAD_DI0_PIN2__AUDMUX_AUD6_TXD,
MX6Q_PAD_DI0_PIN4__AUDMUX_AUD6_RXD,
...
}
(3)Adjust bsp file
Open board-mx6q-sabresd.c ,modify like the following :
static struct platform_device mx6_sabresd_audio_wm8958_device = {
/*Here is sound card divice's name,it should be the same as that of Machine driver*/
.name = "imx-wm8958",
};
static struct mxc_audio_platform_data wm8958_data = {
.ssi_num = 1,
.src_port = 2,
.ext_port = 6, /* Means "ssi2--->aud6 --- >codec"*/
.hp_gpio = SABRESD_HEADPHONE_DET,
.hp_active_low = 1,
};
Regards,
Weidong
Hi,
I am using following command to play audio file
alsa_aplay test.wav
File plays fully but no sound heard.
If i am trying to play file using android music player then i got follwoing error.
W/AudioTrack( 2141): obtainBuffer timed out (is the CPU pegged?)
after song playback completed i got follwoing error.
I/ServiceManager( 2261): Waiting for service media.player...
I/ServiceManager( 2491): Waiting for service media.audio_policy...
I/ServiceManager( 2141): Waiting for service media.audio_flinger...
I/ServiceManager( 2261): Waiting for service media.player...
Any idea where is a bug?
have you try to run alsamixer? may be the volumn is too low so no sound heard.
No I havent tried alsamixer.
Hello,John,
Could you tell me the what type of audio codec is?
Regards,
Weidong
Hi,
Its a normal audio amplifier,
Thanks for this information, I have done the same thing.