Price vs Performance

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Price vs Performance

跳至解决方案
3,212 次查看
salihsonmez
Contributor I

I notice that IMX6 serisi is cheapper than processor with powerpc cores. for example IMX6Dual core is cheaper than P2020. When I compare both as performance ,  P2020 is not extremely powerful as compare with IMX6 dual core. Is there any reason  that I don't notice?

0 项奖励
回复
1 解答
2,994 次查看
Yuri
NXP Employee
NXP Employee

The QorIQ processors are intended for specific (network) applications,

with (relatively) strong technical requirements (environment, reliability, etc)

and (relatively) restricted market.

The i.MX6 (mainly) are intended for general multimedia (mass market)

applications.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,994 次查看
salihsonmez
Contributor I

So , Am I correct, the reason of their price differences are not performance values (Integer and floating point operations). ? It is ımportant for me that I dont  want to ignore or pass over any important performance difference between two processor?

0 项奖励
回复
2,994 次查看
Yuri
NXP Employee
NXP Employee

For network related operations QorIQ performance may significantly exceed i.MX6 one (even for the same Ethernet speed).

0 项奖励
回复
2,994 次查看
salihsonmez
Contributor I

Thanks for quick answer.

0 项奖励
回复
2,995 次查看
Yuri
NXP Employee
NXP Employee

The QorIQ processors are intended for specific (network) applications,

with (relatively) strong technical requirements (environment, reliability, etc)

and (relatively) restricted market.

The i.MX6 (mainly) are intended for general multimedia (mass market)

applications.

0 项奖励
回复