Price vs Performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,155件の閲覧回数
salihsonmez
Contributor I

I notice that IMX6 serisi is cheapper than processor with powerpc cores. for example IMX6Dual core is cheaper than P2020. When I compare both as performance ,  P2020 is not extremely powerful as compare with IMX6 dual core. Is there any reason  that I don't notice?

0 件の賞賛
返信
1 解決策
2,937件の閲覧回数
Yuri
NXP Employee
NXP Employee

The QorIQ processors are intended for specific (network) applications,

with (relatively) strong technical requirements (environment, reliability, etc)

and (relatively) restricted market.

The i.MX6 (mainly) are intended for general multimedia (mass market)

applications.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,937件の閲覧回数
salihsonmez
Contributor I

So , Am I correct, the reason of their price differences are not performance values (Integer and floating point operations). ? It is ımportant for me that I dont  want to ignore or pass over any important performance difference between two processor?

0 件の賞賛
返信
2,937件の閲覧回数
Yuri
NXP Employee
NXP Employee

For network related operations QorIQ performance may significantly exceed i.MX6 one (even for the same Ethernet speed).

0 件の賞賛
返信
2,937件の閲覧回数
salihsonmez
Contributor I

Thanks for quick answer.

0 件の賞賛
返信
2,938件の閲覧回数
Yuri
NXP Employee
NXP Employee

The QorIQ processors are intended for specific (network) applications,

with (relatively) strong technical requirements (environment, reliability, etc)

and (relatively) restricted market.

The i.MX6 (mainly) are intended for general multimedia (mass market)

applications.

0 件の賞賛
返信